Part Number: DS90UB927Q-Q1
Hello! We want to use the LVDS output of the iMX95 (NXP) to connect it to the DS90UB927 serializer, so that it eventually reaches an LCD. To do this we follow this flow: "iMX95 -> LVDS interface -> DS90UB927 serializer -> FPD-link III interface -> DS90UB926 deserializer -> LCD". We have the doubt in the path "iMX95 -> LVDS interface -> DS90UB927 serializer", since we know the rest of the flow works well. Specifically, the doubt comes because the LCD is only 480x272 and the pixel clock we use is 10.8MHz. We know that this is supported by the DS90UB927 serializer (supports range [5MHz, 85MHz]), but we don't know if the iMX95 supports it. Does anyone know? Thank you, Daniel.