I have the next problem, I'm working with TI devices for make a rs485 interface (half duplex) ,
I use a MAX3221IDBR and SN75176BDR. one of the differential channel (channel B)
doesn't output the signal correctly, the output in channel A is inverted but without noise than have
the channel B.
For this reason, I have tried to test only the rs232 interface with the PC and this
worked well, the RS232 signal in the output of the MAX was between -5V and 5V, later,
I have put the SN75176 and the signal in the same point was between -0.8V and 7V.
I really dont understand what happens. can someone help me?