Part Number: DP83867IR
We are observing an issue related to the RX_CTRL hardstrap pin (configured using external 5.76 k ohm pull-up and 2.49 k ohm pull-down resistors as a voltage divider). This issue does not occur 100%, and some boards do not exhibit the problem.
On affected boards, the IC enters a failure state and does not operate correctly. Even when we assert the reset signal, the divided voltage on the RX_CTRL pin remains incorrect.
The only way to recover the device is to perform the following steps:
Remove the external pull-up and pull-down resistors on the RX_CTRL pin.
Measure the RX_CTRL pin to ground using a multimeter in resistance (ohm) mode. The measured resistance initially reads a few k ohm, then gradually increases, eventually rising to approximately 50–60 k ohm.
Reinstall the pull-up and pull-down resistors. After this, the IC resumes normal operation.
This behavior suggests that the multimeter's resistance measurement (which applies a small voltage or current) clears an internal fault condition inside the IC.
We also observed that even after the issue has been resolved, the failure may reoccur if the board is left unused for an extended period of time.
Do you have any insights or recommendations that could help us resolve this issue?