Part Number: TUSB321
Hi Experts,
The datasheet states to use 500k resistor for 1.5A. However, I cannot find one.
What is the minimum and the maximum value that I can use for this? will 510k work?
Regards,
Marvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB321
Hi Experts,
The datasheet states to use 500k resistor for 1.5A. However, I cannot find one.
What is the minimum and the maximum value that I can use for this? will 510k work?
Regards,
Marvin
Hi Marvin,
The 500KOhm resistor is meant to work with the internal PD on the CURRENT_MODE pin to help set the voltage to the mid-level input voltage:

If a 510KOhm resistor will allow the voltage going into the CURRENT_MODE pin to be within that mid-level range, it should be okay.
Thanks,
Ryan
Hello,
Closing thread due to inactivity. If you have any follow-up questions or concerns, feel free to reply.
Thanks,
Ryan