Part Number: ESD321
Hi team,
Regarding the waveform characteristics shown in Figures 5-3 and 5-4 (8kV IEC 61000-4-2 clamp voltage waveform, from I/O pin to GND) in the datasheet (p.6), do they vary significantly across the operating air temperature (TA) range (-40 to +125°C)?
For example, if these waveforms were measured at +25°C, how would the clamping voltage immediately after application (approximately 50V) and the decay voltage 50ns after application (approximately 7V) change at -40°C and +125°C?
https://www.ti.com.cn/lit/ds/symlink/esd321.pdf
Thank you.