Part Number: TCAN1057A-Q1
Hi,
When I used the TCAN1057A-Q1 chip to develop PCAN, the chip could only run up to 4M speed and could not
communicate at 5M and above. The 4M speed communication waveform edge was slow during testing,
and the chip specification stated that it supports up to 8M. Replacing the NXP chip in the same testing environment
worked normally, and the communication waveform edge was normal during testing. Is there any related case or
possible reason for this?
The below is our schematic diagram:

The below is our waveform for 4Mbps speed rate:
- RX;
- TX;
- CANH;
- CANL