Part Number: DS320PR822
I'm currently testing a prototype board with DS320PR822. I use this part for PCIe Gen3/4. I also use this part as a clock (100MHz) mux but it is not working. I configured the redriver on "non PCIe signals" using RX_DET function tied to L0 level, and other signals are in the expected state. The input signal is correct but nothing can be plot on the output.
Here an extract from the schematic:

TThanks for your support.