Part Number: TMDS171
Dear All,
Would you kindly tell us the recommended treatment for the SCL_CTL and SDA_CTL pins of the TMDS171 when using the TMDS171 in "Pin Strap mode" with I2C_EN set to low(I2C_EN/PIN = Low)?
Is it okay to pull up the SCL_CTL and SDA_CTL pins of the TMDS171 to Vcc?
Or does it need to install 2kohm resistors between the SCL_CTL and SDA_CTL pins and Vcc?
We also do not use the TMD171 to communicate with other devices via I2C.
Best Regards,
Hayashi