Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9546A: what different between TCA & PCA

Part Number: PCA9546A
Other Parts Discussed in Thread: TCA9546A

Dear TI,

I saw the 9546 have two kind of title,

one is TCA9546A, and another is PCA9546A,

what's different?

  • Hi Youchin,

    One of the significant differences between the two devices is the supply voltage range. The TCA9546A has a wider operating voltage range of 1.65V to 5.5V, whereas the PCA9546A has a narrower range of 2.3V to 5.5V. This difference in supply voltage range also impacts the high and low input voltage thresholds.

    Thank you,
    Arya