Other Parts Discussed in Thread: TPD7S019
Hello
I want to use TPD7S019 for my VGA connector. I already have a different ESD device on my design and it only contains a zener diode and TVS diode arrays. I am wondering if TPD7S019 requires external AND gates for HSYNC and VSYNC pins. Does the buffer inside the chip do the same thing with the AND gate((((one of the AND gate's pin is connected to 5V and the other is connected to VSYNC or HSYNC pins coming from GPU. The output is connected to a VGA connector))))?
Another thing, I need 33ohm resistor between SYNC line and VGA connector for impedance matching, TPD7S019 provides 15ohm, 55ohm and 65 ohm options. Should I choose the chip with 15 ohm and add 18ohm resistor in series with SYNC_OUT pins?
Thanks for any help.
Emin