Part Number: AM26LV32E-EP
Team,
My customer has the following question:
I am reviewing AM26LV32EMDREP and AM26LV32EIDRG4 as FFF (form, fit, function) replacements for obsolete DS26LV32ATMX/NOPB, and there are some parameters listed in the datasheets that are not defined for the opposite part. Are you able to provide the parameters below if available/applicable? I’m not sure if you’ll be able to provide anything for DS26LV32ATMX/NOPB since it is obsolete, but I wanted to ask and see.
DS26LV32ATMX/NOPB:
Junction to case thermal resistance
Operating virtual junction temperature
Differential input voltage
Common-mode input voltage
High-level output current
Low-level output current
Power dissipation capacitance
AM26LV32EMDREP / AM26LV32EIDRG4:
Junction to case thermal resistance
Output Short Circuit Current
Rise Time (20% to 80%)
Fall Time (80% to 20%)
Thanks,
Aaron