This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: AM2432 PCIe-to-GPMC Bridge: Unexpected Extra FPGA Accesses

Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG

Hello, I have a question regarding the PCIe and GPMC interfaces on the AM2432.
Our current system configuration is Host ⇔ AM2432 ⇔ FPGA.
The Host communicates with the AM2432 via PCIe, and the AM2432 communicates with the FPGA via GPMC.
(The GPMC is configured as 16‑bit address/data multiplexed, asynchronous, single access.)
A portion of the FPGA’s address space is exposed in the PCIe address space so that the Host can access it.
When the Host performs a write to the FPGA, we observe what appears to be three dummy accesses for every single write.
The PCIe packet Length is 4 bytes.
Since I could not attach the waveform image, here is a textual description of the signal behavior. When the Host accesses the FPGA address region, the AM2432 generates four GPMC cycles. During these four cycles, CS, ADV, and AD toggle for all four cycles, but the WE signal is asserted in only one of the four cycles (at a  arbitrary position).
Would you happen to know what might be causing this behavior?
Is it possible that the internal CBASS is converting the transaction into a 64‑bit access or something similar?

That is all. Thank you in advance for your support.

  • Greetings,

    Can you share what software base you are using? Is it Linux, the MCU+SDK, or some custom code specific for your use-case?

    Sincerely,

    Lucas

  • We are implementing it on a custom board based on the Industrial Communications SDK for AM243x – RTOS Version: 2025.00.00.08.

  • Thank you for the information, this will help me find the right resource for this. I have some minor follow up questions as well about the addressing, can you share the details on:

    • What GPMC address ranges (or rather FPGA address range) is the host accessing in the AM2432 when you specifically see this issue? 
    • How have you mapped the address ranges in the PCIe BAR setup? 
    • Does this issue occur at specific addresses or does it occur for any arbitrary address tried?

    Sincerely,

    Lucas

  • What GPMC address ranges (or rather FPGA address range) is the host accessing in the AM2432 when you specifically see this issue?
    >0x50000000~. 

    How have you mapped the address ranges in the PCIe BAR setup?
    > Sorry, I'm not the software engineer, so I don't know the details, but I can share the PCIe settings from sysconfig.
    If more details are needed, I'll ask the software team.

    PCIe Instance : PCIE 0
    Operational Mode : EP mode
    Operation Speed : Gen2
    Number of Lanes : 1
    Reference Clock Mode : External Reference Clock, no SSC
    SRIS Configuration : Disable
    Legacy Interrupt Pin : Pin none
    Number of MSI Vectors : 1
    Inbound Address Translation
    Region Index : 1
    Transaction Layer Packet Type : Memory Type TLP
    Lower Base Address : 0x4000
    Upper Base Address : 0x0
    Lower Target Address : 0x50000000
    Upper Target Address : 0x0
    Region Window Size : 0x0
    BAR Aperture : 16KB
    Bar Configuration : 32bit Mem BAR Non Prefetchable

    Does this issue occur at specific addresses or does it occur for any arbitrary address tried?
    > In our system, the host currently only accesses 0x50001014. When accessing 0x50001014, the addresses transition over 4 cycles as 1010, 1012, 1014, 1016, with WE asserting at the 1014 timing.
    This behavior does not occur during GPMC's standalone write access to the FPGA.

  • Hello ,

    When the Host writes 4 bytes via PCIe to address 0x50001014 (GPMC region), the AM2432 generates 4 GPMC cycles with addresses cycling through 0x1010, 0x1012, 0x1014, 0x1016. The WE signal is asserted only during the cycle at address 0x1014.

    I feel the observed behavior is caused by internal bus width expansion in the AM2432 interconnect.

    The PCIe write transaction passes through the following path:

    PCI → Internal Interconnect → GPMC Controller → External Bus

    The internal interconnect aligns transactions to 64-bit (8-byte) boundaries. When a 4-byte write targets address 0x50001014:

    1. The interconnect aligns to the 8-byte boundary: 0x50001010
    2. An 8-byte transaction is generated with byte-enables indicating only the valid bytes (at 0x1014)
    3. GPMC controller converts the 8-byte transaction to four 16-bit bus cycles
    4. WE is asserted only for the cycle containing valid data (0x1014)

    To confirm this root cause, please perform the following test:

    Test 1: Different Write Sizes from Host :

    │ Host Write Size: 2 bytes │ Expected GPMC Cycles: 4 cycles │ Expected WE Assertions:  1 WE 

    │ Host Write Size: 4 bytes │  Expected GPMC Cycles: 4 cycles │Expected WE Assertions:  2 WE 

    │ Host Write Size: 8 bytes │ Expected GPMC Cycles:4 cycles │ Expected WE Assertions: 4 WE 

    Please share the above test results ..

    Regards,

    Anil.

  • Thank you for your response.
    After checking with the software team, I was informed that the host cannot be changed, so I will close this issue as a device limitation.