Part Number: TUSB8043A
HI,
Regarding the pin settings when connecting an external I2C EEPROM and I2C bus, is the following connection correct?
1. When connecting an external I2C EEPROM (USB hub operates as master)
-> Set SMBUSz/SS_SUSPEND (#39) to Hi and set to I2C Mode
2. When accessing via I2C from an external device (USB hub operates as slave)
-> Set SMBUSz/SS_SUSPEND (#39) to Low and set to SMBus Mode
3. If an external I2C EEPROM is connected, I would appreciate it if you could also tell me how to write the register setting.
Best Regards,
Nishie