Part Number: DP83867ERGZ-S-EVM
Hi,
I would like to report an issue observed with the following setup:
- First laptop connected to a first DP83867ERGZ-S-EVM board via RJ45
- First DP83867ERGZ-S-EVM board connected to a second DP83867ERGZ-S-EVM board via SGMII (SO_P/N to SI_P/N using 25 cm SMA cables)
- Second laptop connected to the second DP83867ERGZ-S-EVM board via RJ45
When running a 1 Gbps Ethernet TCP test using iperf3 in client/server mode, we observe some retries. The frequency of these retries is variable: they may appear after about 12 minutes, after one or several hours, or, in the best case, only after around 16 hours.
If we connect the two laptops directly with a RJ45 cable, without using the DP83867ERGZ-S-EVM boards, no retries are observed (tested over 60 hours).
I have two questions:
- Have you already tested such a configuration?
- Do you have any idea about the root cause of this issue and a possible solution or workaround?
Best regards,
Hermann