Part Number: TCA39306
Hello,
I am considering TCA39306DDFR for my new development work.
Below is the block diagram of my intended circuit.
I have following queries pertaining to above proposed block diagram using TCA39306DDFR
- Do I need to use pull up resistors on I3C bus considering the fact I have two legacy I2C devices?
- If I have to use pull up ressitors on I3C bus, shall I use those pull resistors at 1.8V side or 3.3V side?
Alternatively, you can redirect me to suitable material from where I may get clarification to above technical queries.
Regards,