This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD9491-SEP: IBIS Model

Part Number: THVD9491-SEP
Other Parts Discussed in Thread: THVD1452

Is there an IBIS model for this device?  Specifically need one with 2.5V logic.

Thanks!

  • Hi Connor,

    Unfortunately, we do not have an IBIS model for this transceiver at this time. 

    The closest IBIS model we have is the THVD1452, which is a full duplex transceiver that can also operate up to 50 Mbps. But it is missing the lower VIO reference voltage option.

    Best,

    Ethan