Part Number: TCAN2847-Q1
Dear TI experts,
My customer have a question about thermal via of TCAN28473RHBRQ1.
In the page 226 of datasheet I can find land pattern example as below ;
- Can I use vias which diameter is larger than 0.2mm? Because End customer's recommendation is larger than 0.3mm.
- Can I use more than 12 vias? what is maximum number of vias? is it unlimited?
I am asking it because I saw the description as below.
"For thermally challenging applications, TI recommends that the thermal vias be placed on a pitch of approximately 1,0 mm. Per standard PCB manufacturing capabilities, 0,3 mm diameter drill holes are recommended as a starting point, but a smaller via offers less risk of solder volume loss."
Please check this issue. Thanks.
Best regards,
Chase