This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB5461-Q1: Can I use TUSB5461RGFRQ1 to split all USB data lines (USB2 & 3) into two.

Part Number: TUSB5461-Q1
Other Parts Discussed in Thread: TUSB8041, HD3SS6126

Hi All,

 

Can I use TUSB5461RGFRQ1 to split all USB data lines (USB2 & 3) into two.

I do not need DP 2.1 alt mode.

As I need to drive HD3SS6126 downstream then into TUSB8041.

Or can you recommend a better IC to use?

 

Thanks

 

Matt