This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV31: is the AM26LV31 device RS485 compatible?

Part Number: AM26LV31

is the AM26LV31 device RS485 compatible?

 

please advise

Thank you

Fausto Bartra

  • Based off of the VoD @ 100  ohms, it is not. The minimum VoD required to be RS485 compliant is 1.5V at 54 ohms. 

    From a functionality point of view, it may be possible for it to work on an RS485 bus but it would not be guaranteed and may depend on loading conditions.

    -Bobby