Part Number: TMDS181
Dear TI team:
We are using TMDS181 in order to improve HDMI output. But now we are facing HDMI compliance test fail issue.
Our produce's HDMI out support up to 4K30hz. When it works in 4K mode, the test pass. But when it works in 1080P mode, the single-ended voltage is always below the limit value, while the mask test is pass.
-- in 1080P mode, the lower limit value is 2.7V, but the test value is always about 2.6V. Pls see below pic.

Here is our configuration about TMDS181:
VSADJ=7.06K
PRE_SEL = No Connect
TX_TERM_CTL = 75 to 150 Ω
I have tried to modify transmit termination and swing, it works, but when it pass the single-ended voltage test, the eye pattern mask test will fail.
Please guide us how to modify? Currently, it is operating in GPIO mode, and if need, it can be work on I2C mode.