Part Number: TSWDC155EVM
Other Parts Discussed in Thread: ADC3683EVM,
Dear Texas,
I have a project where I need to sample data out of a sensor. I plan to use an AD3683 at a relatively low frequency of 5 to 10 Msamples / s.
I have ordered the two boards ADC3683EVM and TSWDC155EVM and I manage to perform a capture of input variations.
However, I would like to thouroughly test the interface between the Sensor and the ADC to see if I have injection noise reducing performance of the whole system.
For doing so, I would like to perform a continuous measurement of several hours and retreive data.
1- Is it possible to do something like this through the existing Firmare/Software ?
2- If not, is it possible to provide the existing schematics and firmware of the TSWDC155EVM in order to modify it and perform the continuous measurement ?
Best regards
David Baudin