Part Number: DS125DF111
Good morning TI experts.
I would like some help regarding the optimal configuration for the DS125DF111 chip, so that it can function as a RETIMER on a Xilinx Aurora 64b/66b link at 10.3125 Gbps. At the moment, it seems to work if I select Interlaken2 mode in the SigCon Architect GUI, but I'm not sure if this is the "perfect" configuration. If I set it to "Ethernet," the Aurora link doesn't work. I used the DS125DF111 on a custom board that uses two 10Gbps optical SFP+ .
In the attached photo the link is red (no signal), only because the optical fibers were disconnected:

I would also like to have the optimal configuration for a "10Gbps ETHERNET" fiber optic link.
Thanks,
LM