This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3435-Q1: Review TPS3435CAKAGDDFRQ1 circuit

Part Number: TPS3435-Q1

HI TI Team,

We are using TPS3435CAKAGDDFRQ1 as an Hardware watchdog.We would like you to review our circuitary.We have IGN_INT as an Hardware interrupt and WDG_EN as an Sofware interrupt from Microimage.png

  • Hi Vinyas,

    Is there a pullup resistor on the WDO net? This is an open drain active low output that requires a pullup resistor and voltage.

    Can you confirm my understanding of the circuit is the desired configuration:

    • The WD-EN pin is enabled when the logic level is high and disabled when logic level low. As it is now the watchdog is disabled via R12044 (47kohm) to ground unless a signal is provided on IGN_INT or WD_EN_FROM_VIP.
    • I assume either the top or bottom resistor on SET0 and SET1 will be depopulated. As it is now with all resistors populated SET0 and SET1 are at 0.5*VDD which is a gray area for the logic level.

    Thanks,
    Joshua

  • Hi Joshua,

    Is there a pullup resistor on the WDO net? This is an open drain active low output that requires a pullup resistor and voltage.

    Yes we have an 10k Pullup to P_5V_KA on the other page of schematic.

    The WD-EN pin is enabled when the logic level is high and disabled when logic level low. As it is now the watchdog is disabled via R12044 (47kohm) to ground unless a signal is provided on IGN_INT or WD_EN_FROM_VIP.

    Yes only when IGN_INT or WD_EN_FROM_VIP are triggered the Watchdog is enabled

    I assume either the top or bottom resistor on SET0 and SET1 will be depopulated. As it is now with all resistors populated SET0 and SET1 are at 0.5*VDD which is a gray area for the logic level.

    Yes , we will depop the top resistors 

    ONE MORE QUERY:

    We have the WDI PWM coming from microcontroller in 3V3 power domain. So we were planning to change the circuit as below so to meet the WDI requirement of VIH as minimum 0.7VDD.Do you see any risk as the WDI is edge triggered?

  • Hi Vinyas,

    So long as the BJT is sufficient to pull the voltage level below 0.3*VDD there should be no issue. Schematic looks good.

    Thanks,
    Joshua