Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26C31: Request for T&R Version and Missing Tape Specifications for PN

Part Number: AM26C31

Dear Team,

We require the T&R version for the mentioned PN. At present, Tape Pitch and Tape Width details are missing for most PN data, which is preventing further processing.

Kindly share the required tape specifications to proceed.

Thank you.GE ICE PCBAs_Jerin .xlsx

  • Hi Jerin,

    I see that you are looking at the AM26C31ID and AM26C32ID. Part numbers with "R" in the end of the name mean that they come in a T&R. Since your PN are missing the "R", they come in a tube package, which is why they are missing the tape details. 

    The AM26C31ID and AM26C31IDR are the same device. The difference is that AM26C31IDR comes in T&R. The datasheet describes the T&R details on page 22 for the "R" device. 

    Let me know if that answers your question or if you have any other questions.

    Best,

    Ethan

  • Hello 

    Thanks for the response and support 

    But for some PN we cant able to find the T&R packing and that Pn are not available in - Carrier pack material lookup tool: Carrier pack material lookup | Texas Instruments

    Could you check and confirm if the PN is available or obsolete for eg.XIO2001ZGU 

    Thanks 

  • Hi Jerin,

    It looks like you are using obsolete devices, which is also why XIO2001ZGU does not return anything in the Carrier Pack Material lookup. 

    Please scroll to the bottom of the product page where you can find the active part numbers. For instance, XIO2001IZWSR is active and shows up in the carrier lookup: https://www.ti.com/product/XIO2001 

    Best,

    Ethan

  • Hello 

    Thanks for the mail

    could share the details for the below Pn's that would be really helpful

    POWER SUPPLY 5 VOLTS 306m AMPS 5 VOL REGULATED, 1000V ISOLATION, SO-28 DCR010505UE4
    LOGIC INTERFACE DRIVER QUAD LVDS DS90LV047ATMTC NOPB
    LOGIC INTERFACE RECEIVER QUAD LVDS DS90LV048ATMTC NOPB
    SENSOR TEMPERATURE 3 DIODE INPUT LM83CIMQA NOPB
    IC LOGIC BUFFER-DRIVER 1GATE 74AHC1G125 SOT-353 74AHC1G125DCKRG4
    PROCESSOR DSP, FIXED-POINT, 32 BIT, 400MHZ, 1.05V,1.2V CORE, 1.8V,3.3V IO, 361 PIN PBGA TMS320C6424ZWT4
    IC, PCI-E 2.0 TO PCI TRANSLATION BRIDGE, 1.5 AND 3.3V VCC, LEAD FREE BGA169 PACKAGE - REFERENCE ALSO SIMILAR VARIATION 5400709-2 XIO2001ZGU
    IC, PCI-E 2.0 TO PCI TRANSLATION BRIDGE, 1.5 AND 3.3V VCC, LEAD FREE BGA169 PACKAGE - REFERENCE ALSO SIMILAR VARIATION 5400709-2 XIO2001ZWS

    Thanks

  • Hi Jerin,

    I only support the AM26C31. However, my comments above still apply. For the devices in that list that do not return anything from the Carrier pack material lookup, then it is because those devices are no longer manufactured. I would also double check the formatting. Please the use the exact formatting found on the ti.com product page. 

    If you have additional questions, please create a new E2E question with the specific device name. 

    Best,

    Ethan

  • Hello

    I have check and update with the help of Carrier pack material lookup tool but still i have some doubts could you clarify it

    1. LM83CIMQA/NOPB

    LM83CIMQA/NOPB. identified LM83CIMQAX/NOPB as the SMT tape‑and‑reel version of the same device.

    However, when checking the Carrier Pack Material Lookup Tool, no carrier tape information (such as tape type, tape width, or pocket dimensions) is available, and the tool displays “No search result found” for this part number.

    Kindly confirm:

    • Whether the carrier pack details for LM83CIMQAX/NOPB are available through any other reference/document, or
    • If the carrier pack data is not listed in the tool despite the part being available in tape‑and‑reel.

    2. TMS320C6424ZWT4

     confirmed from the TI website that TMS320C6424ZWT4 is available in tray packaging: www.ti.com/.../TMS320C6424ZWT4

    Despite this, the Carrier Pack Material Lookup Tool shows “No search result found” for this part number.

    Please confirm whether:

    • The absence of search results is due to tray packaging (carrier tape not applicable), and
    • The part is still considered active and not obsolete.

    3. DCR010505UE4

    The part DCR010505UE4 has been identified as DCR011203U/1K, which is available in tape‑and‑reel (T&R) packaging.

    However, similar to the above parts, we are unable to find carrier tape details (tape type, width, or pocket dimensions) in the Carrier Pack Material Lookup Tool, which again returns “No search result found.”

    Kindly clarify:

    • Whether carrier pack details are documented under a different reference, or
    • If the absence of data in the tool does not imply obsolescence of the part.

    Clarification Requested

    Could you please confirm whether a “No search result found” response in the Carrier Pack Material Lookup Tool:

    • Indicates a tooling/packaging data limitation only, or
    • Should be interpreted as the part being obsolete or not recommended for new designs?

    Your confirmation will help us proceed with BOM validation, SMT assembly planning, and lifecycle risk assessment.

    Thank you for your support.

  • Hi Jerin,

    It looks like the carrier pack material lookup does not catch everything. You will need to create a new E2E post tagged with the specific part number to get the correct support.

    Best,

    Ethan