Part Number: AM2434
Other Parts Discussed in Thread: TS3DDR3812, DP83869
Good Morning
I am current working on a design using the AM243x (the ALX package), a TS3DDR3812 mux, and a pair of DP83869's to the EtherNet Phy Layer components. We are planning to use two EtherNet ports so the RGMII1/2 along with the CPSW..etc come into play.
- Are the signals for the MDC and MDIO connected directly between the two DP83869's or must they go from the AM243x pins through a mosfet switcher to each DP83869 separately? One app note said one way, the other said the other way. Or is this switcher internal to the SoC?
- The software team is currently using the LP-AM243x Launchpad eval board. They want to have the EtherNet connections to the same ports on the AM243x on our design as the eval board. I have found the interface to the TS3DDR3812 mux in the Launchpad manual. However, in page 36 (Figure 4-10) it shows the RGMII1/2...etc signals to the mux, and then it references Items 11 and 12 (goes to the SoC). I am unable to find these references to I can verify my connection to the SoC against what they are using on the Eval board. Please assist.
- Also, as a side question, does TI have an option on using one external crystal for the SoC and the two DP83869's through a CDCLC1310 crystal mux or will that cause timing issues?
Thank you for your time.