Part Number: TIOS1013
Other Parts Discussed in Thread: TVS3301, , TSM36A, TSM36CA
Hi Team,
Posting on behalf of our customer.
I am trying to simulate the working of TIOS1013 to better understand the working of nfault pin at different fault conditions. I also want to add TVS3301 to the output pin of TIOS1013 and simulate whether the TVS can keep the TIOS operational during a surge and ensure that the TIOS does not enter any fault condition. I am using PSpice for TI for simulation where I can find the model for TVS3301. But I was not able to find the model for TIOS1013. When I searched in the product page of TIOS1013, I was able to download the IBIS model.
Can I use the IBIS model to simulate the above mentioned circuit? Does the IBIS model have all the information related to TIOS1013 that can be used to simulate it like spice models? If yes, how can I import the IBIS model to PSpice and perform the simulation?
If not, what other options do I have to ensure that the TIOS1013 won't enter fault detection mode during a surge when its output pin is connected to TVS3301?
Regards,
Danilo