This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9535: Need part difference and suggestion.

Part Number: TCA9535
Other Parts Discussed in Thread: TCA9555,

TCA9535RTWR vs TCA9555  which one is better if we are targetting easy design, low current consumption and targetting UL certification.

 

  • The TCA9555 datasheet says:

    The TCA9555 is identical to the TCA9535, except for the inclusion of the internal I/O pull-up resistor, which pulls the I/O to a default high when configured as an input and undriven.

    Whether you want internal pull-up resistors depends on the requirements of your specific circuit.

  • Hello Krishna,

    As Clemens mentioned, the only difference between TCA9535 and TCA9555 is the internal pull-up resistor on the I/O pins.

    Regards,

    Josh