This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: DP83630 with TMS570LC43x – replacing RJ45 MagJack with AFBR-57E6APZ optical module

Part Number: TMS570LC4357
Other Parts Discussed in Thread: LAUNCHXL2-570LC43, DP83630

Hi TI Team,

I am using the LAUNCHXL2-570LC43 / TMS570LC43x board with the onboard DP83630 PHY.

I would like to replace the RJ45 MagJack (J11) interface with an Avago AFBR-57E6APZ fiber transceiver module for optical Ethernet communication.

For initial testing, I have taken the PHY-side signals TD+, TD−, RD+, RD− from J11 and connected them to the Avago module.

Could you please confirm:

- Is DP83630 compatible with this optical module?
- Can the RJ45 section be bypassed/replaced with this fiber interface?
- Is there any reference schematic / recommended coupling and termination network for this connection?

Please let me know if this approach is valid.

Thank you. 

  • Hi Asheeq,

    We never implemented this on practical from our end.

    However, the similar PHY seems to use for fiber optic and succeeded, please refer below thread to understand the same:

    (+) DP83640 - Interface forum - Interface - TI E2E support forums

    And also, we have internal AI and we get some good suggestions from it, you can refer them as well:

    Compatibility Assessment

    • Yes, the DP83630 PHY can work with the Avago fiber module with proper interfacing. The DP83630 has standard differential transmit/receive interfaces that can be adapted to work with the fiber transceiver.

    • The RJ45 section can be bypassed since you're directly connecting to the PHY-side differential signals (TD+/-, RD+/-).

    Important Implementation Considerations

    1. Signal Level Adaptation:

      • The DP83630 PHY uses voltage levels designed for twisted pair Ethernet
      • The Avago AFBR-57E6APZ expects specific signal levels for optical transmission
      • You'll need proper AC coupling and termination
    2. Coupling Network Requirements:

      • AC Coupling Capacitors: Use 100nF capacitors in series with each differential signal line
      • Termination Resistors: Add 100Ω resistors across each differential pair at the receiver side
      • Biasing Network: The Avago module may require biasing resistors to establish proper DC operating points
    3. PHY Configuration:

      • Configure the DP83630 for standard MII/RMII operation
      • Disable auto-negotiation features that depend on copper-specific signaling

    Recommended Connection Approach:

    DP83630 PHY               AFBR-57E6APZ
    ----------- ------------
    TD+ -----||------ 100nF -------→ TX+
    TD- -----||------ 100nF -------→ TX-
    (100Ω across TX+/TX-)
    RD+ ←-----||------ 100nF --------- RX+
    RD- ←-----||------ 100nF --------- RX-
    (100Ω across RX+/RX-)
    --
    Thanks & regards,
    Jagadish.