This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869EVM: Issue with setting up 100Mbps

Part Number: DP83869EVM

Hi,

I have config LED[2:0] = 000 and OP_MODE[2:0] = 100 and have connected the AM62b-P1 board.

Hardware connection looks something like this - 
PC>UMC-GA1F1T>DP83869EVM>AM62b-P1 board.

In this case LED0 & 1 are on, and LED2 is blinking. It works perfectly; I was able to ping the board, but when I connect the BeagleBone Industrial, only the LED2 will blink for 5-10 sec, and then it will turn off.

I thought maybe Beaglebone needed 100 Mbps, so I have set OP_MODE[2:0] = 101: LED0 was on for 3-5 sec and turned off, LED1 was off, and LED2 was blinking for 10 sec and then turned off.

It wasn't able to connect to the BeagleBone at all. Can you help me with this issue?

 

Thank you.