Part Number: DP83869EVM
Hi TI team,
I am currently considering purchasing the DP83869EVM.
My intended use is to evaluate whether this board can be used as both a golden device and a link partner for Ethernet electrical compliance testing of 10BASE-Te, 100BASE-TX, and 1000BASE-T.
I am asking this because the DP83869EVM product page states that the EVM supports copper Ethernet protocols such as 10BASE-Te, 100BASE-TX and 1000BASE-T, and also states that it supports interoperability testing, compliance testing and BER testing.
However, after reviewing SNLA239D and the E2E thread below, I am not clear whether DP83869EVM officially supports the full set of 1000BASE-T compliance-related test modes required for this intended use, especially Test Mode 3 / slave jitter unfiltered:
In that E2E thread, TI states that:
- DP83869EVM does not support slave jitter unfiltered test
- TX_TCLK cannot be provided externally without additional internal jitter
- indirect Test Mode 3 does not give conclusive test result
Also, in SNLA239D, Appendix B does not provide a Test Mode 3 script, and the document states that slave jitter testing cannot be conducted.
Therefore, I would appreciate an explicit official clarification on the following points:
1. Can DP83869EVM officially be used as a golden device for Ethernet electrical compliance testing across 10BASE-Te, 100BASE-TX, and 1000BASE-T?
2. Can DP83869EVM officially be used as a link partner for those same test activities?
3. For 1000BASE-T specifically, does DP83869EVM officially support Test Mode 3 / slave jitter unfiltered?
4. If Test Mode 3 is not officially supported, should the product-page wording be interpreted as supporting only selected compliance tests rather than full compliance coverage?
5. If there is any official limitation document or statement that defines this restriction, could you please point me to the exact document and section?
This clarification is important because it directly affects my purchase decision and my evaluation plan.
Best regards,
Shion Nakagawa