Part Number: DP83867IR
Hello,
We are encountering errors at the physical layer. We are seeing the following type of syslog message from the DPAA driver (linux kernel 5.10.186):
fsl_dpaa_mac 1ae8000.ethernet int0: Err FD status = 0x00080000
We are using a very short cable setup (a few centimeters). We followed the recommendations for register values provided for this type of situation.
However, when we dump the register values, we observe two discrepancies:
address : value from dump -> recommended value
0x0115 : 0xb8bb -> 0x5555
0x0118 : 0x8bf9 -> 0x0771
Is this expected? These registers (like many others mentioned in the recommendations) are not documented in the datasheet, which makes it difficult to understand whether this behavior is correct. Did you have a more exhaustive datasheet, where this fix is described ?
Do you have any recommendations to help us better understand or debug this issue?
thanks a lot,
JCO