Other Parts Discussed in Thread: DS92LV2422, DS92LV2421
I need dc-balanced solution to ser/des random binary data of 18 bits at 62.5MHz clock. Can I use the DS90UR905Q/906Q serdes pair with HS=VS=DE=0 and six unused data lines also grounded?
It wasn't clear from the spec sheet if transitions are required for any reasons on these pins. The spec sheet mentions the chipset is useful for displays up to 1024x768, but I am hoping this is just a max data rate issue rather than some unmentioned transition requirement on HS, VS, and DE.
Thanks,
Deane