This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSB41BA3B-EP: TSB41BA3BTPFPEP vs TSB41BA3FTPFPEP

Part Number: TSB41BA3B-EP

Hi, working with a customert to change from TSB41BA3BTPFPEP to TSB41BA3FTPFPEP for a newer design.  The “B” version  is in their production program, this will be the first project using "F" version.  It appears that these are drop in compatible and that it would not have to make any SW changes to account for swapping to the “F” version.  From what I can tell from datasheet section 13.2.3 which lists the updated features they all seem to be handled by the PHY and are backward compatible.  Can you confirm that should be true and that there are no other potential gotchas to making this update?

 

Thank you!

  • Kannan,

    You are correct, while features have been added to the F version, it was designed to be backwards compatible with access to additional features.

    Please let us know if there are any issues.

    Regards,

    Eric Hackett