Part Number: TL16C550C
Hello,
I would like to inquire about the allowable tolerance for oscillator frequency stability of the TL16C550C.
For reference, the oscillator frequency stability is ±20 to ±100 ppm.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TL16C550C
Hello,
I would like to inquire about the allowable tolerance for oscillator frequency stability of the TL16C550C.
For reference, the oscillator frequency stability is ±20 to ±100 ppm.
Thank you.
Jinho,
We don't really have a spec on the oscillator tolerance. Lower is obviously better since all of the sampling on RX and Tx data relies on this clock. At 100ppm, this seems like there is a 0.01% chance of a error which seems pretty low to me. I would probably say this is acceptable.
-Bobby