This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: TUSB320 DRP with Load switch

Part Number: TUSB320

Hi TI team,

I am looking at using TUSB320 as CC controller for my design requirements mentioned below:

  • My board has a primary 5V power source but should also power up using the Type C port (via UFP mode) when the primary source is absent and I plug a charger. I am ok with 5V 3A power profile.
  • USB storage devices such as Flash drives should work on the Type C port (via DFP mode providing 5V 500mA default) when the primary source is available.

Can you please clarify on the load switch design implementation on how to achieve both requirements?

Regards,

Harsh