This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDP2004: TDP2004 compatibility with PS8483

Part Number: TDP2004

Hello,

Has TI tested the compatibility between the TDP2004 and the PS8483 DP/HDMI retimer ?

We are looking for a suitable solution, and the TDP2004 appears to be a strong candidate.

Thank you in advance.

  • Hi,

    We have not tested the TDP2004 compatibility with PS8483. But with TDP2004 being a linear re-driver, its output will faithfully preserve the the input signal as long as the input signal is within the TDP2004 linearity range, so I do not see an issue of using TDP2004 with PS8483. 

    You can also request a TDP2004 EVM and physically test it with the PS8483.

    Thanks

    David