This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2036 Immediately enters suspend mode

Other Parts Discussed in Thread: TUSB2036

I am having an issue with the TUSB2036 chip. Windows 7 is recognizes that a USB device is plugged in, but calls it 'unknown device' and does not recognize it as a generic USB hub.  When the chip powers on, it immediately enters suspend mode (logic 1 on pin 32 SUSPEND).

The Chip is connected as follows:

NPINT[1:0] = 11 (two permanently attached devices)

NP3 = 1 (only using two ports)

EXTMEM = 1 ( No EEPROM)

DP0PUR (1.5K resistor to DP0)

Xtal1 Xtal2 (connected to 6Mhz resonator)

Mode = 0 (6Mhz Resonator/Crystal)

BUSPWR = 0 (Bus Powered)

OVCUR 1-3  = all tied to 1 (no over-current protection needed)

Reset = connected to RC of 15k and 0.1uF to create reset signal.

What could be causing the chip to always enter suspend mode?

Matthew