Part Number: SN74LV8T244-EP
Hello,
I have a question about the VOL (Low-level Output Voltege) of SN74LV8T244-EP.
In the datasheet, I could found the VOL (@Vcc=5V, IOL=8mA) is 0.3V in the table of section 5.5 (Electrical Characteristic), but it seems that the VOL is about 0.14V (@IOL = 8mA) on VOL vs IOL curves in LOW state; 5V supply(Fig. 5-4).
Which value is correct?
Or, is there a mistake in my understanding of the datasheet?
Thanks.