This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: Ethernet PHY reset issue

Part Number: DP83848K
Other Parts Discussed in Thread: AM623

Hi,

We are developing a linux based system using AM623 processor and DP83848K ethernet PHY with 50Mzha clock from the processor and it using RMII communication.  But we are facing a random ethernet chip initializaton failure in some of the boards means in  sometines first boot it work but next boot it will not work sometines it work after 5-6 reboot. from the u-boot and linux logs we understood during initialization there is a randon communication failure happning with AM623 and DP83848K.  We following https://github.com/TexasInstruments/ti-linux-kernel/blob/ti-linux-6.12.y/arch/arm64/boot/dts/ti/k3-am625-beagleplay.dts reference configuration.

As an experiment, we tried reading the standard registers during the failure condition, but it returned 0xFFFF. We also tried all possible addresses from 0 to 31, but none of them worked in the failure condition.

What are the possible reasons for this random PHY failure? As per our understanding, the DP83848K datasheet states that it has a POR (Power-On Reset) functionality. However, it sometimes fails for unknown reasons. What could be the possible causes of a POR failure?

  • Hi Jomon,

    To preface, DP83848 is an older part with support limited to existing documentation. If there is still an option to switch to a newer device I would recommend using DP83826A. DP83826A is similar in function to DP83848 and is fully supported. Now to address the issue:

    1. Does register access work in cases where the initialization is successful? 

    2. By 'boot' are you referring to a hardware reset or a power cycle of the board?

    3. Is X1 stable on powerup? The powerup timings diagram suggests a stable clock at powerup:

    Best,

    Shane

  • Hi,

    Does register access work in cases where the initialization is successful? 
          On the same board, register access works when initialization is successful. We have already verified this using U-Boot MII commands. However, on the same board, it does not work when initialization fails.

    By 'boot' are you referring to a hardware reset or a power cycle of the board?
         It is a power cycle

    Is X1 stable on powerup? The powerup timings diagram suggests a stable clock at powerup:
         From the DSO analysis it is stable. For an experiment we tried to disconnect the 50 MHz clock line from PHY but still we can able to access the MDIO communication if it in good state.

  • Hi Jomon,

    In the failing state, is DP83848 still able to link up on the MDI? Since there is no register access you may need to check the LED_LINK for this.

    Do you see any differences in the power sequence in passing vs failing states?

    we tried to disconnect the 50 MHz clock line from PHY but still we can able to access the MDIO communication if it in good state.

    To confirm, you're able to disconnect the X1 input of the PHY and it will still respond at some power-ups? I would double check that this clock is provided at powerup and is constantly supplied to the PHY.

    Do you see activity on the MDIO bus in the failing state or is the bus silent?

    Do you see this on all of your boards or only some of them?

    Does replacing the DP83848 PHY have any effect on the behavior?

    For context on my questioning, the fact that the MDIO communication is failing suggests a hardware issue. Since this is power-cycle dependent I'm mostly looking at how the PHY is powered up.

    Best,

    Shane

  • Hi,

    Q. Do you see any differences in the power sequence in passing vs failing states?
        No, we are using the same power procedure for both successful and failed cases.

    Q. To confirm, you're able to disconnect the X1 input of the PHY and it will still respond at some power-ups? I would double check that this clock is provided at powerup and is constantly supplied to the PHY.

         A. Yes, based on our experiments, MDIO/MDC communication works without a 50 MHz clock source. No clock is provided to the PHY during startup, as it is isolated at the hardware level.

    Q. Do you see activity on the MDIO bus in the failing state or is the bus silent?
       A. 
    We observed MDC activity before resetting the PHY. During Linux code analysis, I found that this behavior is normal when using the PHY-level reset method in device tree configuration.

    Also, MDIO communication is multi-node, where the master communicates with different PHY devices and can poll their registers, correct? In that case, will MDIO activity affect the PHY chip?



    Q. Do you see this on all of your boards or only some of them?
        A. 
    The project started around 1.5 years ago. During that time, we used the development version of the board. Many developers worked on it, and both unit testing and system testing were conducted regularly during the development phase. However, we did not face this particular issue. And those board are still working properly.

    Now, we have moved to the production version of the board, with changes to address EMI/EMC issues. This issue has only been observed in the production boards and not all board showing this issue.



  • Hi,

    I have already created an AM623-based thread to discuss this issue. The Linux-based discussion is ongoing, and I am adding this here for reference.

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1637182/am623-how-to-change-the-ethernet-phy-reset-sequence-with-cpsw-davinci-mdio-driver

  • Hi Jomon,

    If the previous iteration of the board did not have this issue, I'd like to know what was changed moving to the production version. It seems this fixed EMI issues but is now causing this communication issue.

    Best,

    Shane