This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1021-Q1: Schematic review

Part Number: TUSB1021-Q1

USB-MUX.pdf 

  • Input: USB 3.1 Gen2 high-speed signals from SoC (TX/RX differential pairs)
  • Application: Automotive IVI System (USB data switching / routing)
  • Output: Routed USB 3.1 Gen2 signals to USB Type-C connector (up to 10 Gbps)

Kindly let me know if any additional application details are required for this schematic review, or if any corrections or additional components are needed in the design. Also, if you have any layout recommendations, kindly let me know.