This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB319-Q1: Product_Selection

Part Number: TUSB319-Q1

I would like to have a USB C power advertising device with the following attributes:

1) Advertises to load (battery charger) a 1p5A current cabability 

2) No USB data transfer needed (or wanted)

3) no digital programming (SPI,I2C ect). Resistor pull up or pull down desired

4) surface mount only

5) 5VDC power supply

"TUSB319-Q1 USB Type-C DFP Port Controller" might be the solution, but I observe no connections to DATA(+) or DATA(-).   

 

Please advise