Part Number: SN65LVCP408
Other Parts Discussed in Thread: DS25CP102
Hi, Experts.
If the Output of SN65LVCP408 can be directly connected to LVDS input? And how to connect LVDS output to the input of SN65LVCP408?
Regards
Powell
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVCP408
Other Parts Discussed in Thread: DS25CP102
Hi, Experts.
If the Output of SN65LVCP408 can be directly connected to LVDS input? And how to connect LVDS output to the input of SN65LVCP408?
Regards
Powell
Hi Powell,
You should be able to provide an LVDS input to SN65LVCP408 since it's input threshold is +/-50mV and LVDS typically swings +/-350mV across a 100Ohm load. I would recommend AC-coupling if you are using the internal VBB bias. However, if you are wanting to connect the VML output of SN65LVCP408 to an LVDS receiver, you will need to check the receiver datasheet to make sure you aren't violating it's max voltage limits since VML outputs a higher voltage than LVDS. Since you are dealing with LVDS inputs and outputs, it would be better to use a dedicated LVDS switch like DS25CP102 to avoid these issues.
Regards,
Matt