This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044-Q1: DCC slow transient pulse

Part Number: TCAN1044-Q1
Other Parts Discussed in Thread: TCAN1044A-Q1,

Dear

In the datasheet for model "A", I see a different value listed compared to that for model without "A". 

Transient voltage per ISO 7637-3 - DCC slow transient pulse.

TCAN1044A-Q1 (SLLSFJ3D – AUGUST 2023 – REVISED OCTOBER 2024) : ±30 V

TCAN1044-Q1 (SLLSF17D – AUGUST 2019 – REVISED MARCH 2025): ±85 V

Are these actually two different values, depending on the model, or is one of the two datasheets out of date?

 

Thanks

  • Hi Roberto,

    Yes, these are two different devices with two different data sheets as specified.

    Note that most applications do not require as high as 85 V and would strongly recommend the newer device with a more robust HBM spec instead, if feasible, thanks.

    Best Regards,

    Michael.