Part Number: TCA9548A
Dear TI
What is Vo(sw)(Switch output voltage) ?
For examle ,Vcc =1.8V typ 1.1V .
Is this meaning that Vol max become 1.1V??
Takeshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9548A
Dear TI
What is Vo(sw)(Switch output voltage) ?
For examle ,Vcc =1.8V typ 1.1V .
Is this meaning that Vol max become 1.1V??
Takeshi
Vo(sw) is not relevant for I²C communication.
There is no VOL because the TCA9548A is an analog switch. The connection between the SCL/SDA pins and any active channel behaves like a resistor for low-level signals; see the RON specification.
Dear Clemens Ladisch
Thank you very much for replying me.
Do you mean Vo = Ron × Io ?
For example, If Io = 10mA and Vcc= 1.8V ,Vol become 700mV max?
Takeshi
Hi Takeshi,
Your output voltage will be input voltage minus the drop that occurs across the switch (Vo = Vi - Ron*I). Turning on the switch is creating a channel for your input signal to travel through. Your output signal's voltage will be largely dependent on your input voltage and equivalent resistance seen at the output with some voltage drop due to the on resistance of the switch. Your system will most likely not have the same current as the test conditions used in the Ron section of the datasheet, so be sure to account for that.
-Hunter
Hi Hunter
thank you very much for your answer.
I could understand with you explanation.
-Takeshi