Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Hi,
I am using the Ethernet PHY DP83869HM in my new design.
I configure the PHY to Media Converter mode (1000Base-T to 1000Base-X) by strap pins OPMODE[2,1,0]=100 according to Table 7-12 "Functional Mode Strap Table" in PHY data sheet.
It works fine but I have some LINK issues when remote Host (connected to this PHY by RJ45) is being powered-up of rebooted.
At Table 7-19 "1000M Media Strap Table" I see that pin LED_0 is used as starp pin for "Fiber Auto Negotiation" or "Fiber Force Mode".
Since the PHY is configured to "1000Base-T to 1000Base-X" it means that always one side of the PHY is connected to copper and one side to fiber optics.
Can you please explain the meaning of this strap pin and when is correct to use "Fiber Auto Negotiation" or "Fiber Force Mode".
Best Regards,
Moshe