This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: Level Translator for One-Wire

Part Number: TXS0102

Hi Team,

I am usig one-wire interface in my design. Whether TXS0102 level translator can be used for the level conversion from 3.3V to 1.8V for one-wire interface.

Thanks,

Shifali N

  • Hi Shifali,

    Yes TXS0102 supports open drain signaling. Please refer to Recommended Operating Conditions of the datasheet to ensure proper function of the device. This device also has internal pullups conveniently populated so external pullups are not needed.

    Regards,

    Jack