Part Number: TCA4311A
Other Parts Discussed in Thread: TCA9511A,
| TCA4311ADR |
| fall time of both SDA and SCL signals |
| rise time of both SDA and SCL signals |
| data hold time |
| data set-up time |
| Maximum junction temperature |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Surampudi,
I recommend using the TCA9511A, as the TCA4311A has a major errata which is the "missing ACK".
The TCA9511A is p2p and drop-in to the TCA4311A.
The TCA9511A is a buffer and not an I2C target device. The timing requirements must be met by the system level design which is a factor of the bus capacitance and pull-up resistor selection.

Data hold and data set-up times are not required by the TCA9511A since this device is a buffer and not a target device.
Maximum junction temperature for TCA9511A is TJ(max) = 130 C
Regards,
Tyler