Other Parts Discussed in Thread: TCA9509
Hi,
As per datasheet for TCA9509, low level output current (IOL) is given as max 10uA only on A side as shown below.
It is given that no external pull ups are required on A side. What will happpen if there is an external pull up also present on I2C lines on A side? As per my understanding, this device sinks 1mA through internal 200Ohm pull down when driving the I2C lines Low on A side driving the lines to ~0.2V and if I have an external pull up also, current sink through this resistor will increase and V(OL) level may increase.
But due the specs given in datasheet max current is 10uA and I am not sure if extra current due to external pull ups will damage the IC.
Actually I have bought OVERO FIRE COM for OMAP from Gumstix which has 4.7k pull ups on I2C lines and I can not remove those resistors on all COMs especially during production.
Can anyone from TI tell me that extra pull ups of 4.7K to 1.8V (~0.38mA current) can damage the IC or not
VIni