This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: Clarification on Partial Networking / Selective Wake-Up Behavior and Configuration Sequence

Part Number: TCAN1145-Q1

Hi Ti Team,

After modifying the logic, I observed the following behavior during Partial Networking / Selective Wake-Up testing, and I would like to cross-check whether this behavior is expected.

Observation:

  1. I configured the Selective Wake-Up settings and then shut down the power supply.
  2. Turn on Power Supply, then I transmitted a valid CAN wake-up frame from the CAN bus.
  3. In this case,when i Send Valid Frame then INH pin became HIGH and RxD Pin low, which appears to indicate a successful wake-up event.

Then I repeated the test with a different condition:

  1. Again, I shut down the power supply.
  2. Re-ran the code and transmitted an invalid CAN frame.
  3. In this scenario, the INH pin remained LOW and RxD Pin has 3.3v.

Based on this observation, my understanding is that:

  • A valid configured wake-up frame correctly triggers the INH pin High and RXD pin Low.
  • An invalid frame does not trigger wake-up and keeps INH LOW and RXD pin high.

Could you kindly confirm whether this is the correct expected behavior for Partial Networking / Selective Wake-Up operation?

Additional Clarification Required:

I also wanted to understand why the following registers/configurations are not additionally required in this flow:

  • Mode Control Register
  • Wake Pin Configuration
  • Pin Configuration Register

Currently, selective wake-up appears to work without explicitly configuring these registers, so I would appreciate clarification on:

  • Whether these registers are internally defaulted to the required state, or
  • Whether they are only needed for specific use cases/features.

Current Sequence Followed:

The current flow implemented in the software is approximately:


void TCAN_operationDeviceMode(void)
{
uint8_t reg;
initQSPI_TCAN1145();
TCAN_Init();/*Already Here I set the configuratipon For the Standby */
/**************Added Only For Wake Up Frame*************/
/* Enable selective wake */

TCAN_WriteReg(TCAN_REG_INT_ENABLE_1,(1 << 6) ); // Enable bit 6 (CANINT)
/*Configure wake filter */
// MODE RELATED (0x11, 0x12) ---
TCAN_WriteReg(TCAN_WAKE_PIN_CONFIG, 0x00); // 0xFFWAKE pin disabled / default
TCAN_WriteReg(TCAN_REG_PIN_CONFIG, 0x00); //0x1c RXD/nINT default

// WUF FILTER ---
TCAN_ConfigWakeUpFilter(0x123, TCAN1145_ID_11BIT, 0xFF, NULL, FALSE);

//FRAME DETECTION (MANDATORY) ---
TCAN_WriteReg(0x44, 0xDC);//0xDC
TCAN_WriteReg(0x45, 0x00);
TCAN_WriteReg(0x46, 0x1F); // threshold
/* commit SWCFG */
TCAN_WriteReg(0x47, 0x80);
/*Clearing Bits */
TCAN_WriteReg(TCAN_REG_INT_1, 0xFF); // Clear all bits in INT_1 (0x51)
TCAN_WriteReg(TCAN_REG_INT_2, 0xFF); // Clear all bits in INT_2 (0x52)
TCAN_WriteReg(TCAN_REG_INT_3, 0xFF); // Clear all bits in INT_3 (0x53)
TCAN_WriteReg(TCAN_REG_INT_GLOBAL, 0xFF);

/* NOW enter sleep */
TCAN_EnterSelectiveWakeSleepMode();

/* wait */
Delay_sec(0.01f);
}

void TCAN_ConfigWakeUpFilter(uint32_t can_id, uint8_t id_len, uint8_t dlc, uint8_t *data_pattern, bool mask_enable)
{
int i;
uint8_t wuf_cfg = 0x00;

if (id_len == TCAN1145_ID_11BIT)
{
uint8_t sw_id3;
uint8_t sw_id4;

sw_id3 = (uint8_t)((can_id >> 6) & 0x1F);
sw_id4 = (uint8_t)((can_id << 2) & 0xFC);

TCAN_WriteReg(TCAN_REG_SW_ID1, 0x00);
TCAN_WriteReg(TCAN_REG_SW_ID2, 0x00);
TCAN_WriteReg(TCAN_REG_SW_ID3, sw_id3);
TCAN_WriteReg(TCAN_REG_SW_ID4, sw_id4);
}
else
{
uint8_t id3 = (can_id >> 16) & 0xFF;
id3 |= (1 << 5);
TCAN_WriteReg(TCAN_REG_SW_ID1, (can_id >> 0) & 0xFF);
TCAN_WriteReg(TCAN_REG_SW_ID2, (can_id >> 8) & 0xFF);
TCAN_WriteReg(TCAN_REG_SW_ID3, id3);
TCAN_WriteReg(TCAN_REG_SW_ID4, (can_id >> 24) & 0xFF);
}

uint16_t std_mask = 0x000; // exact match

uint8_t mask4;
uint8_t mask_dlc_bits;

mask4 = (std_mask >> 3) & 0xFF;
mask_dlc_bits = (std_mask << 5) & 0xE0;

TCAN_WriteReg(TCAN_REG_SW_ID_MASK1, 0x00);
TCAN_WriteReg(TCAN_REG_SW_ID_MASK2, 0x00);
TCAN_WriteReg(TCAN_REG_SW_ID_MASK3, 0x00);
TCAN_WriteReg(TCAN_REG_SW_ID_MASK4, mask4);

wuf_cfg |= mask_dlc_bits;

if (dlc != 0xFF)
{
wuf_cfg |= ((dlc & 0x0F) << 1);
}

if (mask_enable && data_pattern != NULL)
{
wuf_cfg |= 0x01;
}

TCAN_WriteReg(TCAN_REG_SW_ID_MASK_DLC, wuf_cfg);

if (mask_enable && data_pattern != NULL)
{
for (i = 0; i < 8; i++)
{
TCAN_WriteReg(TCAN_REG_DATA0 + i, data_pattern[i]);
}
}

}

Could you also kindly review whether this overall sequence is correct for Partial Networking implementation?

Thanks & Regards,
Anil Kumar

 

  • Hi Anil,

    Based on this observation, my understanding is that:

    • A valid configured wake-up frame correctly triggers the INH pin High and RXD pin Low.
    • An invalid frame does not trigger wake-up and keeps INH LOW and RXD pin high.

    This is correct. 

    I also wanted to understand why the following registers/configurations are not additionally required in this flow:

    • Mode Control Register
    • Wake Pin Configuration
    • Pin Configuration Register

    I am not sure I fully understand your question. The MODE_CNTRL register is needed to enter Sleep mode (where SW is active). However, changing MODE_CNTRL is not needed after entering Sleep mode. TCAN1145 automatically enters Standby mode after a valid WUF occurs. 

    WAKE_PIN_CONFIG is not needed to be configured. You can see that the default values mean that the WAKE pin works without manual register adjustment. 

    PIN_CONFIG is just further device customization. The device functions normally, but specific features can be adjusted. Both WAKE_PIN_CONFIG and PIN_CONFIG do not need to be adjusted for SW.

    Please note that we do not do full code reviews as this would take too much time for each customer. But if you encounter issues or unusual problems, then you can reach out.

    But I do have a couple notes on your code comments. 

    TCAN_WriteReg(TCAN_REG_INT_ENABLE_1,(1 << 6) ); // Enable bit 6 (CANINT)

    Just note that INT_ENABLE_1 just enables the INT_1 mask. The CANINT function is not actually disabled, only the interrupt flag is disabled. 

    TCAN_WriteReg(TCAN_WAKE_PIN_CONFIG, 0x00); // 0xFFWAKE pin disabled / default

    I see your comment that "Wake pin disabled." Note that this pin cannot technically be disabled. However, if you do not need it, you can simply tie it to GND on the schematic. Or you can set the WAKE pin to a pulse that it will never see. 

    Best,

    Ethan