Part Number: TCAL9538
Hi Team,
I have a few questions regarding the TCAL9538PWR device.
I am planning to use the I2C IO expander to drive an 7 segment display and would like clarification on the maximum output drive current per Port when operating at a 3.3 V supply.
Additionally, I noticed in the datasheet that the device includes internal pull-up and pull-down resistors with a minimum value of 70K. Could you please clarify whether these ports are capable of driving LEDs with minimum 3-5mA drive current